Hi, it is difficult question and I am afraid it is above possibilities of basic support.
To start off I want to mention that we try to avoid recommending specific devices to customers for memory and other external components. Because of the large number of choices out there it is impossible for us to have hands-on experience with all of them, and we don't want to recommend devices that we haven't used ourselves. We are at least indirectly recommending devices by including them on our EVBs and reference designs. So in most cases our best recommendation is to use the devices we have used or at least find something similar that will meet your specific needs.
However one the document explicitly says that "it is apparent that even with a fast DDR2 SDRAM, the largest panel supported with full color encoding is WVGA (800 x 480, c. 33 MHz)." what could be good hint. It is true that MPC5645SDEMO board uses LPDDR1 but it also uses smaller TFT panel. Thus I would pay your attention to DDR2 memories.
In the following link you may see excel tool (originally tailored to MPC5121E that is however using almost the same DRAM controller), showing in the bottom tabs certain DRAM devices so could possibly use it as starting point for your DRAM selection:
https://www.nxp.com/docs/en/user-guide/MPC5121EQRUGAD.xls
Regarding QSPI memory -
MPC5645S Microcontroller Reference Manual, Rev. 8, Section 35.8 shows all supported instructions codes for 4 selected vendors (Winbond / Spansion / Macronix / Numonyx chosen by QSPI_MCR[VMID]) producing (or developing) QuadSPI memories at the time of developing MPC5645S MCU (somewhere around year 2010). As I know Spansion has been acquired by Cypress, Numonyx by Micron, Winbond and Macronyx probably stays under same name.
2 x Spansion S25FL064P has been used with MPC5645SDEMO board, mentioned memory manufactures could possibly help you to choose proper device, I expect newer devices are backward compatible.
Hope it helps a bit