NXP ls1088ardb booting from sd card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP ls1088ardb booting from sd card

543 次查看
Rusanya_T
Contributor I

NOTICE: UDIMM 18ADF2G72AZ-2G6E1
ERROR: Board parameters no match.
ERROR: Failed matching board timing.
ERROR: Found training error(s): 0x2100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platfor_def.h
ERROR: mmap_add_region_check() failed. error -22
ERROR: mmap_add_region_check() failed. error -22
NOTICE: BL2: v1.5(release):LSDK-20.12
NOTICE: BL2: Built : 04:35:28, Dec 11 2020
this is the output when I try to boot the ls1088ardb board using sd card. how to fix this error

RusanyaT
0 项奖励
回复
0 回复数