Hi,
I have used PN7150 module integrated with android Nougat 7.1.2.
I have followed below mentioned procedure provided by NXP.
This works fine for our platform to read the NFC cards, Here I want to know how to enable a sound while a card read.
Will it has the support with these patches ? or What is the procedure to enable the sound ?
Please provide the solution as soon as possible.
I think the Android is running on a MCU/MPU. The beep sound should be controlled by the MCU/MPU. e.g. the beep sound from a buzzer. The beep sound from the buzzer can be controlled by GPIO output 1/0.
Hi jimmychan,
We have external speaker connected to our board & it has the capability to play the audio files.
Can you please mention with audio file will be played when the NFC read & where it is located ?
This will help us for the further debugging.
Thanks for the reply.
Can you please share the information related to the GPIO (number) which is connected to the buzzer & the connection procedure ?
Which MCU or MPU you used for running Android? You should check your Android SDK and porting guide . e.g. add the GPIO support in device tree file for your MPU/MCU. This is not related to PN7150.
Hi jimmychan,
Thanks for the reply.
We are using Qualcomm APQ8909 for our project. Can you please share PN7150 DTS with buzzer configuration ?