MRF6V2150N impedance in the frequency range 414 to 442 MHz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF6V2150N impedance in the frequency range 414 to 442 MHz

1,829 Views
marcos_rodrigue
Contributor I

Dear, as mentioned above, I need the 's' parameters or the impedance for this frequency range, Thanks.

0 Kudos
1 Reply

1,754 Views
LPP
NXP Employee
NXP Employee

You can evaluate source and load impedances using high power non-linear model of MRF6V2150N.

For your pleasure, I performed load-pull and source pull simulation using ADS tool. The results are attached. Question drain current was set 450mA. Lambda/4 Tline was used as drain bias.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos