Default Configuration for SJA1105TEL Ethernet Switch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default Configuration for SJA1105TEL Ethernet Switch

5,367件の閲覧回数
arun_panangala
Contributor II

Hello,

We are developing a custom hardware solution with the SJA1105TEL which connects a PHY, SBC and a FPGA with RGMII interface. Is there a default configuration provided by NXP that we can upload  using the sja1105-tool to get the system running with basic functionality like forwarding packets from the PHY to the SBC ?

Kind Regards
Arun.

0 件の賞賛
返信
5 返答(返信)

5,252件の閲覧回数
hmulyono
Contributor I

Hi Platon,

I have found the Python file you were referring to:  /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py.

I found out that the following parameters depend on the board layout, so they need to be changed for my application:

  • xMII_MODE[0..4]
  • PHY_MAC[0..4]

Is there any other board-specific (e.g. port dependent) register I need to change? If I just changed the above two parameters, would it work?

The block diagram of my system is available below. I just want my three devices (i.e. Jetson Xavier AGX, ethernet jack, and the other MAC device) to communicate.

Regards,

Hermawan Mulyono

EDIT: I should have replied to @bpe 's post directly, but I could not post two messages in an hour.

blockdiagram.JPG

 

0 件の賞賛
返信

5,236件の閲覧回数
bpe
NXP Employee
NXP Employee

To be clear: there is no one-fits-all configuration for SJA1105 switch. What  example_configs/pyScripts/ directory provides, is a set of more-or-less typical configurations for a  reference. You can start with the one that is close to what your board needs, but it cannot save you reading the documentation. Refer to AH1601 for  board and interface specific parts of the switch configuration.

Best Regards,

Platon

 

 

0 件の賞賛
返信

5,320件の閲覧回数
bpe
NXP Employee
NXP Employee

If on your board all switch connections are RGMII, you can start with /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py. Thie file is part of the configuration tool SW package. Details can be found in AH1601

 

Hope this helps,
Platon

5,316件の閲覧回数
arun_panangala
Contributor II

Hi Platon,

Thank you for your reply. Where can I find the configuration tool SW package ? Does this require us signing an NDA ?

Regards,
Arun.

0 件の賞賛
返信

5,277件の閲覧回数
bpe
NXP Employee
NXP Employee

This tool is part of SJA1105 Application Board Package 1.4

 

Regards,
Platon

0 件の賞賛
返信