Tire Pressure Monitoring System (TPMS) - FXTH87

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tire Pressure Monitoring System (TPMS) - FXTH87

Tire Pressure Monitoring System (TPMS) - FXTH87

Demo Owner Mike Stanley

 

Tire Pressure Monitoring Systems (TPMS) help drivers with precise direct tire pressure measurement by providing individual tire readings – including the spare. NXP's world’s smallest, lowest-power, with highest memory for customer use TPMS is highly integrated with a pressure sensor, temperature sensor, accelerometer, MCU and a transmitter. Watch Mike Stanley explain the pressure sensor readings, temperature sensor display and the accelerometer/motion readings. These readings are time based periodic measurements where the data is given as an output to the driver.

 

Features

  • Simulation that portraits the TPMS as if it were inside the vehicles tires and sending reports to the vehicle's display unit about tire pressure
  • Module has the following: Pressure sensor, accelerometer, temperature sensor, low-frequency radio, Microcontroller

 


Featured NXP Products


Links

ラベル(1)
コメント

I can not find the demo ,how Can I get it?

How I can get Development kit or Reference design information of FXTH87 based TPMS? Thank you!

評価なし
バージョン履歴
最終更新日:
‎07-01-2014 08:45 AM
更新者:
NXP Employee