Guide to designing antennas for the NTAG I2C plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Guide to designing antennas for the NTAG I2C plus

Guide to designing antennas for the NTAG I2C plus

This post entry provides a guide to designing antennas for the NTAG I2C plus. This article has been structured as follows:

How the NTAG I2C plus works

The NTAG I2C plus is what we call a connected NFC tag. It combines a memory, a passive NFC interface and a contact I2C interface. Additionally, it has more features such as:

  • A field detection pin, to send a wake-up signal to a connected MCUntag i2cplus.png
  • The Energy harvesting, able to power external devices
  • The SRAM, a memory without writing cycles limitation
  • The pass-through mode, for fast data exchange between interfaces
  • Memory access control options, available from both NFC and I2C interfaces
  • And the originality signature, to protect your brand against clones

As such, it supports bidirectional communication between an NFC-enabled device and the host MCU and it is an ideal solution for Industrial applications, IoT nodes, meters, consumer electronics and accessories among others. 

To enable the NFC interface, the chip needs to be connected to an antenna coil using the two dedicated antenna pins. How to design this coil is the main goal for today.

NTAG I2C plus antenna design files

The NTAG I2C plus support package includes development kits, demo apps, sample code, application notes, and, the design files of the Class 4 PCB antenna, and the Class 6 Flex antenna, which are available for direct and free download from the website. ntag psp.png These design files

include:

  • The schematics 
  • The Gerbers
  • The BoM

Therefore, if you do not have any antenna size or shape constrains in your application, the easiest is to just copy & paste these reference antennas.

On the other hand, if you need to design your custom antenna, NXP also offers a coil design Excel sheet to help you. I will talk more about it along the article.

Basic antenna theory for NTAG I2C plus tags

The NTAG I2C plus is an 8-pin package, with:

ntag equivalent circuit.png

  • The field detection pin
  • The Vout pin
  • The I2C serial clock and data Iines to the MCU
  • The ground
  • The VCC
  • wo antenna pins


NTAG I2C plus electrical input capacitance

The NTAG I2C plus equivalent circuit can be represented with:

  • A resistor, representing its current consumption
  • And a parallel capacitor, representing the chip internal capacitance

For the NTAG I2C plus, this capacitance is 50pF for both the 1k and 2k memory versions. Precisely, the chip capacitance is the most important factor for the antenna tuning.

Antenna coil electrical equivalent circuit

The antenna coil itself is a resonant circuit with an input impedance. The electrical equivalent model of the antenna coil consists of:

antenna coil equiv circuit.png

  • An inductance
  • A capacitance
  • And some resistive losses of the loop antenna itself.

The actual impedance value depends on: 

  • The antenna material
  • The thickness of the turns, mainly affecting the resistance 
  • The distance between the windings, mainly affecting the capacitance
  • The number of turns, mainly affecting the inductance
  •  And the nearby environment

Tag with an NTAG I2C plus electrical equivalent circuit

When the NTAG I2C chip and the antenna coil are assembled, we can consider a parasitic resistance and capacitance generated by the connections between the chip and the antenna. This parasitic impedance depends on the assembly process used and the antenna material. 

tag equivalent circuit.png

As a result, what we can observe in the schematic of the figure is that the NTAG I2C plus capacitance together with the parasitic connection capacitance and the antenna capacitance forms a resonance circuit with the inductance of the antenna

coil.  

The self-resonance frequency of a system is given when the imaginary part of the circuit equivalent impedance is null, and the system is only purely resistive.

Considering the antenna loop inductance, the parallel equivalent capacitance and the parallel equivalent resistance of the tag, the resonance frequency and the quality factor of the tag can be calculated by these formulas.

fr formula.png


Antenna design procedure for NTAG I2C plus tags

The antenna design procedure for the NTAG I2C plus tags is: 

  1. Design the antenna coil. This is about the antenna specs in terms of number of turns, track width, spacing, shape, etc according to your application requirements.
  2. Characterize the antenna coil and find its R, L, and C parameters.
  3. Calculate the parallel capacitor value required to adjust the tag resonant frequency
  4. Assemble the calculated capacitor and measure the results. If the results are not accurate enough, fine-tune the capacitor value, assemble and measure again as needed.


Design the antenna coil 

As part of the ISO14443 standard, six PICC antenna classes are defined. Per each of the antenna class, the physical characteristics and dimensions are defined. For instance, Class 1 is the largest, with a size comparable to the size of a regular credit card, and Class 6, which is the smaller one. In addition, Class 3 to Class 6 define two antenna shapes: a rectangular and a circular one. However, tag manufacturers are not constrained to conform to any of these dimensions. Therefore, its use is optional and rather intended to improve interoperability. As such, you may consider using these antenna sizes as a reference for your designs.

coil calculation sheet.png

The major parameter of the antenna coil is the inductance. This inductance can be estimated based on geometrical parameters and the material properties such as:

  • The diameter for a round antenna or the overall length and width for a rectangular shape.
  • The track width
  • The gap between track
  • The thickness
  • And the number of turns

To avoid cumbersome formulas, NXP offers you an Excel-based coil calculation tool to estimate the inductance of rectangular and circular antennas. This tool uses some parameters related to the material used and the antenna dimensions. And with it, it estimates the antenna inductance for you. Typically, the coil design steps include:

  • An estimation of the electrical parameters, like the operating frequency and the chip capacitance
  • The definition of the target inductance, we define the dimensions, the track width, the gap between track, the thickness, etc that achieves our target inductance.
  • The production of prototypes. Based on the matrix run, with different inductance values deviated between 10-20% plus and minus the original value.
  • Characterization of the coil prototypes. Based on this characterization, select the one with the best parameters for your application.  If needed, you can execute a second matrix run, with new prototypes, based on the first results.

Measure the antenna coil parameters

The antenna characterization can be done using a network analyzer connected to the antenna pads, isolated from the rest of the circuit. For our case, a low-end solution, such as the miniVNA PRO is sufficient. This device is cheap compared with the high-end devices like Agilent but still, accurate enough for our needs. 

miniVNA.pngAs a remark, it is fundamental that this characterization is done with the antenna placed at its final mounting position, so that all environment effects, like metal plates or others, are considered.

Calculate the resonant capacitor value

We use a network analyzer to measure the system resonant frequency after connecting the NTAG I2C plus to the antenna coil. As I explained before, the self-resonant frequency of the tag is given when the system is purely resistive. Most likely, the actual resonant frequency will not be 13.56MHz as we would like, but some other value. If that is your case, calculate the system capacitance at the current resonant frequency based on the equation derived from the NFC tag equivalent circuit shown previously.

Current fr.pngAt this point:

  • We know the current resonant frequency
  • We know the antenna inductance, because we measured it before with the network analyzer
  • And, as design parameter, we define the target resonant frequency

With this data, we can use once again, this formula to calculate which is the resulting capacitance that would make our tag resonate to our target resonant frequency. Knowing the required total capacitance and the actual capacitance, we can calculate the extra capacitance missing. This is given by this formula:

Capacitance res.png

Regarding the target resonant frequency, for single tag operation, a tuning slightly above 13.56 MHz would lead to maximum read-/write distance. However, due to manufacturing tolerances, a nominal frequency up to 14.5 MHz would still operate well.

vna fr.png

Assemble and measure resonant frequency

Therefore, the last steps are:

  • Solder the capacitor in parallel
  • Connect the network analyzer
  • And measure the new resonant frequency 

If the resonant frequency measured is not the target one, repeat the process by fine tuning the capacitor value.  If the frequency is higher than expected, you can increase the capacitor value. On the other hand, if the frequency is lower than expected, you can decrease it.

Example: Tuning for a 54x27mm PCB antenna

Based on a real lab exercise, this section illustrates the steps to adjust the tuning of an antenna for the NTAG I2C plus.

As described before, we need to start by characterizing our antenna coil. In this lab exercise, we have used a PCB antenna of 54 by 27 mm and, we have connected our miniVNA PRO to the antenna pads. The results that we have obtained from this measurement are that our PCB antenna has an inductance around 895 nH.

Measuring antenna coil.png

After characterizing the antenna coil:

  • We have soldered the NTAG I2C plus chip to this PCB antenna.
  • Right after, we connect again the miniVNA PRO to measure the actual resonant frequency. 

Measured fr.png

In this case, it returns a resonant frequency near 24 MHz. Using the formula, we calculate that the tag capacitance at 24 MHz is almost 50 pF. Note that, the actual capacitance is basically the chip capacitance as the antenna and connection capacitance is usually not impacting significantly.

Obviously, a resonant frequency of 24MHz is way too high for a ISO14443 NFC tag like our NTAG I2C plus. Therefore, we need to add some capacitance to the system so that we can bring this resonant frequency down. As an example, for this lab exercise, we are adjusting the tag to around 13.6 MHz, intentionally a bit higher than the NFC operating frequency. With a target resonant frequency to 13.6MHz and an antenna inductance is around 895nH,  the result is that the tag needs a total capacitance of around 153 pF. This means that we need to solder an extra capacitance of 100pF to bring down the resonant frequency.  So we go to our component box, and select the closer commercial value (100pF).

resonance capacitor calculation.png

As a last step, it is worth to measure how well adjusted is our system after adding the 100pF. We connect the miniVNA to the system including the IC, the antenna and the 100pF. Now, the results obtained are that the resonant frequency is 13.8 MHz. In our case, we consider this as good enough. However, you are always free to repeat this process as many times as needed until you obtain the accuracy that you need.

Resulting fr.png

Summary

The antenna tuning steps for the NTAG I2C plus that we followed are:

  1. Design the antenna coil. You can use the NXP reference antennas or design your own antenna coil using the NXP Excel-based calculation tool.
  2. Measure the antenna coil. Use a network analyzer connected to the antenna pads, without any other circuitry
  3. Calculate the extra capacitance. Measure the current resonant frequency, and we calculate the extra capacitance needed to achieve the desired operating frequency.
  4. Solder and measure. If the results are sufficient, you are done. Otherwise, repeat the process with a new capacitance value

As you can see, the antenna tuning process is quite straight forward. Basically, it is a matter of adjusting the capacitance of the tag until the operating frequency is the right one.

Further information

You can find more information about NFC in:

Video recorded session

On 25 July 2018, a live session explaining this topic was delivered. You can watch the recording here:

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎07-25-2018 05:35 AM
更新者: