Enhancement- 5G + ARM Edge Server

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enhancement- 5G + ARM Edge Server

Enhancement- 5G + ARM Edge Server

Overview

 

The 5G era ushers in changes to the wireless industry and new benefits to end-users. One change is a new partitioning of network-infrastructure functions, dividing the once-monolithic base station into three pieces: the radio unit (RU), distributed unit (DU), and centralized unit (CU). Associated with one or more RUs, the DU performs upper-layer PHY and media-access functions. It shares characteristics of both standard Linux computers and real-time systems and may be deployed in the field.

NXP demonstrated at the 2020 Consumer Electronics Show a working 5G system, including a DU highlighting how the Layerscape LX2160A processor addresses these requirements. This 16-core device integrates multiple high-speed PCI Express interfaces and Ethernet ports running up to 100Gbps, delivering the needed computational performance and I/O in a power-efficient envelope. NXP also showed how its Layerscape Access programmable baseband processors can help enable fixed-wireless access designs for the customer premises, small cells, repeaters, in-home wireless links, and accelerators for CU systems. These programmable devices help mobile operators quickly deploy open radio-access networks. NXP has solutions from the antenna to the processor.

Diagram

pastedImage_3.png

 

NXP Products

Product Name
QorIQ LX2160A Development Board | NXP 
QorIQ® LS2088A Development Board | NXP 
No ratings
Version history
Last update:
‎10-27-2020 09:42 AM
Updated by: