why i cannot get the total 18 bytes data? now i can get only 14 bytes data for Mifare plus first authentication.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why i cannot get the total 18 bytes data? now i can get only 14 bytes data for Mifare plus first authentication.

1,112 Views
xiongqinghua
Contributor I

why i cannot get the total 18 bytes data? now i can get only 14 bytes data for Mifare plus first authentication.

now  i can get the following data stream at the Mifare plus card first authentication.

+++1111-2::MifarePlusReader_Clrc663_FirstAuth()---- datanum=14,errorReg=-34888

++++1111-3::MifarePlusReader_Clrc663_FirstAuth()----Response Data:
0x12 0x90 0x0e 0xe0 0xe0 0x47 0x3e 0x52 0x21 0x90 0x7c 0x09 0xc6 0xcf
++++1111-4::MifarePlusReader_Clrc663_FirstAuth()---- datanum=14,errorReg=0,statusreg=0

the first 0x12 may be the data number for response!!! the second 0x90 may be the status code!!! the following may the  16 bytes random data,but now the random data has only 12 bytes.why?

Labels (1)
0 Kudos
Reply
1 Reply

1,014 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,


As you might know, there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement) and placed in DocStore, you might find there some useful documents and some libraries that might help you with the usage of some readers with the MIFARE Plus, could you please follow this guides?


Docstore tutorial part 1: User Registration|NXP 

Docstore tutorial part 2: portal usage|NXP 


Also, you will need to contact one of our distributors available in the Distributor Network|NXP to help you through the NDA process.


Regards,

Estephania

0 Kudos
Reply