I use PN532 work with ISO14443typeB card,But no work;
I used the "InlistPassive Target"comment.
In the Manual
how can I know whether my pn532 demo support Type PCD funtionality.
the number on chip is:
5321 06
cs0063
05
tsd0091
Hello,
I have problems reading 14443B tags, like credit cards.
It seems that other persons have the same problem.
Is there any specific operation to do ?
I tried:
InListPassiveTarget with various parameters.
Implementing InAutoPoll with these parameters:
0x00 : Generic passive 106 kbps (ISO/IEC14443-4A, Mifare and DEP), 0x01 : Generic passive 212 kbps (FeliCa and DEP), 0x02 : Generic passive 424 kbps (FeliCa and DEP), 0x03 : Passive 106 kbps ISO/IEC14443-4B, 0x04 : Innovision Jewel tag, 0x10 : Mifare card, 0x11 : FeliCa 212 kbps card, 0x12 : FeliCa 424 kbps card, 0x20 : Passive 106 kbps ISO/IEC14443-4A, 0x23 : Passive 106 kbps ISO/IEC14443-4B, 0x40 : DEP passive 106 kbps, 0x41 : DEP passive 212 kbps, 0x42 : DEP passive 424 kbps, 0x80 : DEP active 106 kbps, 0x81 : DEP active 212 kbps, 0x82 : DEP active 424 kbps.
Specifying custom values in SRAM registers (Writeregister 0x08):
Addresses : 0x6302 (CIU_TxMode) et 0x6303 (CIU_RxMode).
Any hint would be appreciated !
Hi,
Our PN532 only has one version, it is no problem to support Type B PCD!
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------