using a pn7462 with multiple smartcards via tda8026

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using a pn7462 with multiple smartcards via tda8026

1,604 Views
dennisblauhut
Contributor II

Hello,

i'm looking for an example for the OM27462CDK evaluation board to communicate with the PN7462  to the TDA8026 slot extender to address smartcards. i'm able to communicate via i2c to the extender, but i'm unable to configure the iso 7816 uart correctly and don't understand the examples of the eval board completely because some part of the firmware are directly in the rom and hard to understand how to config the uart.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,320 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to Um314511 - UM10858 PN7462 HW User Manual (1.1) available under NDA in DocStore.

 

I hope this helps.

Regards,

Ivan.

0 Kudos
Reply