using a pn7462 with multiple smartcards via tda8026

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

using a pn7462 with multiple smartcards via tda8026

1,684 次查看
dennisblauhut
Contributor II

Hello,

i'm looking for an example for the OM27462CDK evaluation board to communicate with the PN7462  to the TDA8026 slot extender to address smartcards. i'm able to communicate via i2c to the extender, but i'm unable to configure the iso 7816 uart correctly and don't understand the examples of the eval board completely because some part of the firmware are directly in the rom and hard to understand how to config the uart.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,400 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to Um314511 - UM10858 PN7462 HW User Manual (1.1) available under NDA in DocStore.

 

I hope this helps.

Regards,

Ivan.

0 项奖励
回复