spi connection and antenna problem for MFRC52

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

spi connection and antenna problem for MFRC52

324件の閲覧回数
wael_fakher
Contributor I

I designed a PCB that integrates an ESP32 and an MFRC522 RFID module. However, the ESP32 was initially unable to communicate with the MFRC522 until I reduced the SPI communication speed to 200 kHz. Even then, the reader was still unable to detect RFID tags.

Additionally, I need the MFRC522 to support three external antennas via IPEX connectors.

I would appreciate guidance on improving my design to ensure stable communication between the ESP32 and MFRC522, and to properly support external antennas.

please see my pcb design 

0 件の賞賛
返信
1 返信

306件の閲覧回数
RafaR
NXP Employee
NXP Employee

Hello wael_fakher

 

We're sorry, but this section of the community is focused on other types of sensors.

We can’t provide help for that family in this section. Please check the next community.

https://community.nxp.com/t5/RFID-NFC/ct-p/RFID-NFC

 

Have a great day and best of luck.

0 件の賞賛
返信