Hi,
i am trying to integrate PN7150 NFC module to my android board. I am integrating drivers to Android Pie version by following AN11690, which is officially available. i have followed the steps of integration given AN11690 and build it but unable to enable the functionality of NFC in Settings. Can someone help me doing this needful.
Thanks
Hello Jimmychan
i have same problem. unable to integrate with android 8.1.0.
i follow this document AN11690.pdf. first it says i need to add repo init. so i add this command ;
repo init -m LINUX/android/.repo/local\_manifest/nxpnfc\_manifest.xml
Downloading Repo source from https://chromium.googlesource.com/external/repo
remote: Counting objects: 265, done
remote: Total 7291 (delta 4910), reused 7291 (delta 4910)
Receiving objects: 100% (7291/7291), 2.65 MiB | 0 bytes/s, done.
Resolving deltas: 100% (4910/4910), done.
fatal: manifest url is required.
here i include my error log.
can you give advice.
Thanks,