lcrc663用于伟根接口

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lcrc663用于伟根接口

980 Views
臣柱宣
Contributor I

你好,请问lcrc663能否支持wiegand协议?我看数据手册只有

ISO/IEC14443A/MIFARE
ISO/IEC14443B
FeliCa
ISO/IEC15693/ICODE
ICODE EPC UID
ISO/IEC 18000-3 mode 3/ EPC Class-1 HF 这几种,并没有看到支持wiegand协议,谢谢

0 Kudos
1 Reply

884 Views
Kan_Li
NXP TechSupport
NXP TechSupport

wiegand协议和ISO 14443A这些协议不是一个概念吧,wiegand一般是指数据存储的格式,https://www.nxp.com/docs/en/application-note/AN10957.pdf?fsrch=1&sr=2&pageNum=1 


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos