is JCOP/J3A081 supports int data type?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is JCOP/J3A081 supports int data type?

1,765件の閲覧回数
PPS74
Contributor I
Hi,
 
I am using latest eclipse JCOP tools for java card applet development.  I need to store big integer values in a card so I have used the INTEGER data type (int) for balance in my applet.  it is compiling without any error but getting error 6A80 on uploading the CAP file into JCOP J3A081/J2A... cards. I have tried all combinations of GP 2.1.1, GP 2.2.1, JDK 2.2.2, JDK 3.0.4 library but getting the same error.
 
I would like to know that int data type variables and JCint library are supported by J3A081 and J2A... cards? if yes please do needful to resolve the issue. 
 
Please have a look on applet source code in attached screenshot.
 
Note: if I remove int data type variable and JCint references then no error comes
 
0 件の賞賛
返信
1 返信

1,736件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi, 

 

This product is a non Mass Market product, please contact your local Disty or NXP sales representative for further support.

Thanks for your patience and understanding!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信