importing SDK-64F into McuXpresso IDE workspace For CLEV6630B Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

importing SDK-64F into McuXpresso IDE workspace For CLEV6630B Library

1,164 Views
chennai2chn
Contributor I

Dear Sir,

Please Support  importing SDK-64F into McuXpresso IDE workspace  For CLEV6630B Library Issues.

CLEV6630B working fine with Given NFC Reader Library function with LPC1769 MCU.

Our objective is to interface CLEV6630B to K24F (myfare classic 1k cards).

Before that we are trying to import K82F library to FRDM-K64F .

*We followed the procedure of importing NFC READE library from K82F TO K64F-”HOW TO PORT THE NFC READER LIBRARY TO K64F” given by NXP

*While importing SDK-64F into McuXpresso IDE workspace :

below error is coming

Fig 1: K64F SDK Format ( Attached )

Fig 2: K82F SDK Format ( Attached )

while importing k64F-sdk itself we are facing path error

SDK version : SDK_2.6.0_FRDM-K64F

to avoid this one, instead of SDK we are importing Example code. Anyhow we are facing lot of problems. Please guide us to solve the above problems and K24F controller also.

Thanks in Advance

Tags (1)
0 Kudos
Reply
1 Reply

1,112 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Chennai,

I am sorry, but the pictures you attached are real low resolution, is it possible to provide a higher resolution or just test of the error message?

BTW, I have tried to import sdk for K64 and K82 in the same time, looks like they can work well together.

pastedImage_1.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply