i need an ISO15693 reader demo board that i can measure precise RSSI with for a proof of concept i am doing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i need an ISO15693 reader demo board that i can measure precise RSSI with for a proof of concept i am doing

698 Views
davidmitchell
Contributor I

I am hoping there would be a GUI already available for the reader demo board front end IC that i can simply enter in a command or click and get the RSSI info from a tag in the field of the reader IS easily for a quick proof of concept i am doing for a potential customer.  I just need something simple and easy off the shelf to do this with that requires no or very little software development.  Please help!

Thanks!

Dave

0 Kudos
1 Reply

471 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Dave,

Yes, there is such kind of reader board (CLRC663) available, and GUI "PCSerial" as well.

When you connect it with PC via serial port, you may send commands to that board, please download the PCSerial from http://www.nxp.com/documents/software/119121.zip , its UM can be found from http://www.nxp.com/documents/user_manual/119221.pdf , and we also provide example scripts for reference, there is a RC663_ISO15693_Inventory.jcf in http://www.nxp.com/documents/software/210910.zip, which should be useful for you as a starting point.

Please refer to http://www.nxp.com/products/identification-and-security/nfc-and-reader-ics/nfc-frontend-solutions/hi... for more details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos