When I use the document of AN11646 which i want to test the OM5577/PN7120S kit, after i write the image of OM5577-PN7120S_BBB_Linux_demo_v1.1 into the BeagleBone Black , and then i want to connect the board via SSH over USB with PuTTY. I enter 192.168.7.2 as the host address,and the PuTTY show me the prompt "login as :" and i type root and press enter . But it shows me Access denied and i can not login the system. Can you tell what can i do to login the system
Hi,
The password should be for linux OS on raspberry board.
you can try the user and password:
user: pi
password: raspberry
If not logging in normally, you can check user' guide of "raspberry pi" or ask provider for help!
Have a nice day!
Best Regards,
weidong sun