bidirectional and transparent communication capability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bidirectional and transparent communication capability

544 Views
hong_zhang
Contributor I

Hi

I am looking for a NFC IC with bidirectional and transparent communication capability. Detail please see the attached file.

Please advise.

Thanks

0 Kudos
3 Replies

428 Views
hong_zhang
Contributor I

Thank you very Jorge

What is theNT3H2111/2211 development kit parts number?

Thanks

Hong

0 Kudos

428 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Hong Zhang,

You can look at the NTAG I2C Plus explorer board. Below is the link:

OM5569-NT322E | NTAG I2C plus Explorer Kit | NFC|NXP 

Regards!

Jorge Gonzalez

0 Kudos

428 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Hong Zhang,

According to your system diagram, the requirement is to have a communication bridge between the MCU and a host NFC reader (PC/smartphone). For this task the best fit would be the NTAG I2C Plus family (NT3H2111/NT3H2211). This IC has a contact interface (I2C) to connect the MCU and a contactless interface (NFC) to interact with an external reader. Please find more details in the product page and in the product presentation in the next links:

NT3H2111/2211|NXP 

NTAG I2C plus - Your entryway to NFC|NXP 

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos