aspi#nxp5442 and NXP MIFARE Classic 1k - C# support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

aspi#nxp5442 and NXP MIFARE Classic 1k - C# support

2,779 次查看
fredit
Contributor I

Hello, I’m looking for solution to get Smart Card ID (Serial Number) over NFC.

Device: Zebra tablet Windows 10

System device: aspi#nxp5442#1#...{fb3842cd-..-4b0761139ae9} visible as NXP NearFieldProximity Provider.

My Smart Card:  NXP MIFARE Classic 1k  (ISO 14443-3A)

Programming language: C#

When I’m use Microsoft ProximityDevice library I can attached to events  DeviceArrived, DeviceDeparted but it is not possible get Card ID. I’m tried use PcscSdk from Microsoft but still not work. Looks like this library works on the Smart Card device but I don’t see this device in Device manager. Maybe I need additional drivers or you have dedicated library for this system device.

Thank you for help.

标签 (1)
0 项奖励
回复
1 回复

2,098 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, as mentioned in the case, we do not have any library for that device. Since you are able to detect the presence or the absence of the card, the problem is not the driver but the library. In this case please contact Microsoft for more information related to reading the UID.

Thank you for your comprehension.

Best regards,

Ivan.

0 项奖励
回复