Wrong detection of RFID for PN71506 on Multiple Tap.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wrong detection of RFID for PN71506 on Multiple Tap.

269 Views
Ganesh_G
Contributor I

Hello Sir,

 

I have two IC for RFID Tag reading IC PN71501 and PN71506. I am using Linux kernel version 5.4 in that for NXP diver i am using nxp-pn5xx/pn5xx_i2c and the library is libnfc_nci_linux-1.so.0.0.0

 

          On PN7501 RFID Tag is working fine for multiple Tags, on every tag it shows the correct value of tag for multiple cards. With the same environment for IC PN71506 it not working correctly. For Multiple tag scan it shows previously id tag continuously for every next new tag scan for 7 to 8 times randomly, after that it's scan correctly and again showing the same tag info for every next tag scan.

 

void onTagArrival(nfc_tag_info_t *pTagInfo)

{

    framework_LockMutex(g_devLock);

 

    if(eDevState_WAIT_ARRIVAL == g_DevState)

    {

        DEBUG_PRINT("\n===== NFC Tag Detected =====\n\n");

       // When we are coping the idtag, we are getting the same id tag information, as we are actullay tapping the differnet id tag,

 

        memcpy(&g_TagInfo, pTagInfo, sizeof(nfc_tag_info_t));

        g_DevState = eDevState_PRESENT;

        g_Dev_Type = eDevType_TAG;

        framework_NotifyMutex(g_devLock, 0);

    }

    else if(eDevState_WAIT_DEPARTURE == g_DevState)

    {

        memcpy(&g_TagInfo, pTagInfo, sizeof(nfc_tag_info_t));

        g_DevState = eDevState_PRESENT;

        g_Dev_Type = eDevType_TAG;

        framework_NotifyMutex(g_devLock, 0);

    }

    else if(eDevState_EXIT == g_DevState)

    {

        g_DevState = eDevState_DEPARTED;

        g_Dev_Type = eDevType_NONE;

        framework_NotifyMutex(g_devLock, 0);

    }

    else

    {

        g_DevState = eDevState_PRESENT;

        g_Dev_Type = eDevType_TAG;

    }

    framework_UnlockMutex(g_devLock);

}

 

We have added some debug prints in below file in this library source code to dubug above issue.

File name  : yocto/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/nxp-nfc/0.1-r0/git/src/service/interface/NfcTag.cpp

Function Name : void NfcTag::setNfcTagUid (nfc_tag_info_t& tag, tNFA_ACTIVATED& activationData)

Code changes are blow,

 

void NfcTag::setNfcTagUid (nfc_tag_info_t& tag, tNFA_ACTIVATED& activationData)
{
    switch (mTechParams [mActivationIndex].mode)
    {
    case NFC_DISCOVERY_TYPE_POLL_A:
    case NFC_DISCOVERY_TYPE_POLL_A_ACTIVE:
    case NFC_DISCOVERY_TYPE_LISTEN_A:
    case NFC_DISCOVERY_TYPE_LISTEN_A_ACTIVE:
        NXPLOG_API_D ("%s: tech A", "NfcTag::setNfcTagUid");
    NXPLOG_API_D("%s: enter, tag_uid=%d tag_uid_len=%x", "NfcTag::setNfcTagUid",
                 mTechParams [mActivationIndex].param.pa.nfcid1, mTechParams [mActivationIndex].param.pa.nfcid1_len);
        tag.uid_length = mTechParams [mActivationIndex].param.pa.nfcid1_len;
        memcpy(tag.uid, &mTechParams [mActivationIndex].param.pa.nfcid1, tag.uid_length);
    NXPLOG_API_D("%s: enter, tag_uid=%x tag_uid_len=%x", "NfcTag::setNfcTagUid",
                 tag.uid, tag.uid_length);

 

 

Please see the highlighted logs below for above debug print,

[2024-07-05 17:04:50.929] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.974  NxpTml:     PN54X - I2C Read successful.....
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.974  NxpNciR:     len =  23 > 61051401808000FF010904000423371116010800000000
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.975  NxpTml:     PN54X - Posting read message.....
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.975  NxpHal:     read successful status = 0x0
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.975  NxpHal:     NxpNci: RF Interface = MIFARE
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.976  NxpHal:     NxpNci: Protocol = MIFARE
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.976  NxpHal:     NxpNci: Mode = A Passive Poll
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.976  NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=23
[2024-07-05 17:04:51.277] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.976  NxpFunc:    nfaConnectionCallback: event= 5
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.977  NxpFunc:    checkforTranscation: enter; event=0x5 transaction_data.current_transcation_state = 0x0
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.977  NxpFunc:    other event clearing flag
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.977  NxpFunc:    checkforTranscation: exit; event=0x5 transaction_data.current_transcation_state = 0x0
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.978  NxpFunc:    nfaConnectionCallback: NFA_ACTIVATED_EVT: gIsSelectingRfInterface=0, sIsDisabling=0
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.978  NxpFunc:    NfcTag::setActivationState: state=2
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.978  NxpFunc:    NfcTag::IsSameKovio: enter
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.979  NxpFunc:    NfcTag::discoverTechnologies (activation): enter
[2024-07-05 17:04:51.292] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.979  NxpFunc:    NfcTag::processNotification (Activation): RF disc_id=01; protocol=80, mNumDiscList=8
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.979  NxpFunc:    Mifare Classic detected
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.979  NxpFunc:    processNotification (activation): NumTechList = 9 sel_rsp=0x8
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.980  NxpFunc:    NfcTag::processNotification; mNumTechList=a
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.980  NxpFunc:    NfcTag::discoverTechnologies (activation): index=0; tech=1; handle=1; nfc type=80
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.980  NxpFunc:    NfcTag::discoverTechnologies (activation): index=1; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.980  NxpFunc:    NfcTag::discoverTechnologies (activation): index=2; tech=1; handle=1; nfc type=80
[2024-07-05 17:04:51.308] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.980  NxpFunc:    NfcTag::discoverTechnologies (activation): index=3; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.319] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.981  NxpFunc:    NfcTag::discoverTechnologies (activation): index=4; tech=1; handle=1; nfc type=80
[2024-07-05 17:04:51.319] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.981  NxpFunc:    NfcTag::discoverTechnologies (activation): index=5; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.319] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.981  NxpFunc:    NfcTag::discoverTechnologies (activation): index=6; tech=1; handle=1; nfc type=80
[2024-07-05 17:04:51.319] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.981  NxpFunc:    NfcTag::discoverTechnologies (activation): index=7; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.319] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.982  NxpFunc:    NfcTag::discoverTechnologies (activation): index=8; tech=1; handle=1; nfc type=80
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.982  NxpFunc:    NfcTag::discoverTechnologies (activation): index=9; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.982  NxpFunc:    NfcTag::discoverTechnologies (activation): exit
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.982  NxpFunc:    NfcTag::createNativeNfcTag: enter
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.983  NxpFunc:    createNativeNfcTag: Selected: index=9; tech=8; handle=1; nfc type=80
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.983  NxpFunc:    NfcTag::setNfcTagUid: tech A
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.983  NxpFunc:    NfcTag::setNfcTagUid: enter, tag_uid=b6f9ac37 tag_uid_len=4
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.983  NxpFunc:    NfcTag::setNfcTagUid: enter, tag_uid=ae1f0740 tag_uid_len=4
[2024-07-05 17:04:51.634] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.984  NxpFunc:    nativeNfcTag_onTagArrival: notify tag is ready
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.984  NxpFunc:    NfcTag::createNativeNfcTag: exit
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.985  NxpTml:     PN54X - Read requested.....
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.985  NxpTml:     PN54X - Invoking I2C Read.....
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.986  NxpFunc:    presenceCheckThread: enter
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.986  NxpFunc:    doPresenceCheck
[2024-07-05 17:04:51.648] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.986  NxpFunc:    doPresenceCheck: sCurrentConnectedHandle= 01
[2024-07-05 17:04:51.649] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.986  NxpFunc:    Calling EXTNS_MfcPresenceCheck
[2024-07-05 17:04:51.649] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.987  NxpExtns:   Mfc_PresenceCheck status = 0x3a
[2024-07-05 17:04:51.649] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.987  NxpExtns:   Error Sending msg to Extension Thread
[2024-07-05 17:04:51.665] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.987  NxpFunc:    doPresenceCheck: NFA_RwPresenceCheck Wait..
[2024-07-05 17:04:51.665] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.988  NxpFunc:    NfcAdaptation::HalWrite
[2024-07-05 17:04:51.665] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.988  NxpTml:     PN54X - Write requested.....
[2024-07-05 17:04:51.665] Jan  8 13:05:47 STCA60B8E9FEE EVOCApp[597]: 2024:01:08-13:05:46.988  NxpTml:     PN54X - Invoking I2C Write.....

 

 

Please find the attached mpu log file for your for detail logs. Here also we are getting same id tag information, for different id tag tapping.

Please suggest where else in the source code we can add the futher debug prints to root cause the issue.

0 Kudos
Reply
1 Reply

235 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @Ganesh_G 

Firstly, I would say sorry, PN7150X is a customized product, and the related design resources are not public, including me, also can't see anything, so it is difficult to provide further support to you, please understand. As for the same environment you mentioned that PN71501 works well but PN71506 does not, it is recommended to check that where is the difference between PN71501 and PN71506, perhaps there will be clues.

0 Kudos
Reply