Workaround for intermittent PN7150 reset after sending start discovery request?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Workaround for intermittent PN7150 reset after sending start discovery request?

935 Views
anthony_asterisk
Contributor II

During operation I sometimes get a reset notification after sending a start discovery command.

The reset shows reason code is A3.  Before the reset an I2C request to start discovery had been sent.

[00:00:34.962,000] <info> nfc: NCI message rx'ed in state 11
[00:00:34.962,000] <info> nfc: 60 00 02 A3 00 |`....

0 Kudos
Reply
3 Replies

831 Views
anthony_asterisk
Contributor II

I am developing on a custom board developed with a Cortex-M4 processor.  The software is bare-metal, there is no software package.  Since the processor is also supporting several other peripherals a custom driver has been implemented that avoids blocking for long periods.  The provided example code does not appear to handle this error case.

0 Kudos
Reply

831 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies. We recommend that you first start with our software and hardware before moving to a custom project.

Thank you for your comprehension.

Regards,

Ivan.

0 Kudos
Reply

830 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Could you please provide us with the following information:

1. Are you working with the evaluation board?

2. Which host MCU are you working with?

3. Which software package?

Regards,

Ivan.

0 Kudos
Reply