Why short range for pn532 in desfire.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why short range for pn532 in desfire.

1,268 Views
annu0412
Contributor II

Why PN532 has short range for desfire ev1 card?When i tap mifare card it can read it from 3cm distance but for desfire i have to tap very close sometime i need to push to antenna.

Tags (1)
0 Kudos
4 Replies

911 Views
annu0412
Contributor II

Hi Vicente

Thanks for your reply.

I bought PN532 board with antenna, how can i calibrate my antenna in this case?

I am a beginner Please help.

0 Kudos

911 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Can you tell me the board part number?

Thanks

0 Kudos

911 Views
annu0412
Contributor II

This is the board pic attached.

How can i get the part number?

Regards

Anurag

911 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Probably you have some problem with the antenna calibration.

You can check the application note AN1445

http://www.nxp.com/documents/application_note/AN1445_An1444.zip 

Regards

Vicente

0 Kudos