Where can I get sample tags with SLIX-S ICs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I get sample tags with SLIX-S ICs?

1,113 Views
thederek
Contributor I

Hello,

   I am working on a reader for specifically the SLIX-S IC. I've seen the ICs available for purchase but no sample tags (complete with antenna etc; suitable for easy testing). Where can I purchase these? It can be from NXP or a Partner; whichever is easiest to purchase.

Thank you,

Derek

0 Kudos
Reply
2 Replies

1,082 Views
thederek
Contributor I

Hello, thank you but this was not helpful. I contacted several of these companies and they don't have SLIX-S based tags. We are investigating using the SLIX-S in a high volume consumables application. But we need tags to use for software development. Where can we buy SLIX-S based tags? For software development we don't care about size, we need to verify that the security works for the application first.

0 Kudos
Reply

1,111 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello @thederek .

You can order the sample tags via the partners as the links.

URL:https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS.

Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply