Hello,
I understand from the demo app on the explorer kit that everything except the NDEF message to be displayed on the screen is sent across the NFC interface (between the NTAG I2C plus and the android phone app) is not NDEF formatted.
My use case is that I want to be able to send some chunks of data or commands back and forth between the tag (with a host micro-controller) and an NFC phone in pass-through mode.
Question is, when and why should I use NDEF encapsulation of the data to be exchanged?
Hi,
the NDEF message format provides a good way to structure messages to be exchanged between devices. At the end it is about you to decide if the NDEF format helps in your particular application, or if it is easier for you to define your own format.
HTH,
Michael
Clear. I could choose to use the NFC chip in the pass-through mode as a modem exchanging custom formatted data with the custom application on the reader side. If there is some information that I need all the NFC certified devices to be able to read without having any additional app installed, I must use NDEF.
Exactly.