Verfication of operations on HTRC110 in contact with HITAG S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Verfication of operations on HTRC110 in contact with HITAG S

956 Views
RemiZHANG
Contributor I

I am trying to read some data with the help of HTRC110 in communication with HITAG S. I use the microcontroller stm32 to communicate with the htrc110. I would like to make sure if the communication works in the following way: Initialization of HTRC110- WriteTag mode to send the UID Request to the HITAG S- ReadTag to receive the data from the transponder. 

The problem is that I do not fully understand what the transparent mode means.

 

Thanks in advance for your reply!

Labels (2)
0 Kudos
1 Reply

935 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

When the transparent mode is being used  the transponder data is directly presented at DOUT with a delay from RX to DOUT depending on the demodulator filter settings.

 

Maybe you can check the Read/write devices based on the HITAG® read/write IC HTRC110   for more details on this on the reading part ,

 

Hope this helps

 

Regards,
Estephania

 

0 Kudos