I am trying to read some data with the help of HTRC110 in communication with HITAG S. I use the microcontroller stm32 to communicate with the htrc110. I would like to make sure if the communication works in the following way: Initialization of HTRC110- WriteTag mode to send the UID Request to the HITAG S- ReadTag to receive the data from the transponder.
The problem is that I do not fully understand what the transparent mode means.
Thanks in advance for your reply!
Hello,
When the transparent mode is being used the transponder data is directly presented at DOUT with a delay from RX to DOUT depending on the demodulator filter settings.
Maybe you can check the Read/write devices based on the HITAG® read/write IC HTRC110 for more details on this on the reading part ,
Hope this helps
Regards,
Estephania