Use the package NxpNfcRdLib in PN7462AU-FW_v05.02.01_Full to join the PN7462AU_ex_phExRf project can not find the following function

cancel
Showing results for 
Search instead for 
Did you mean: 

Use the package NxpNfcRdLib in PN7462AU-FW_v05.02.01_Full to join the PN7462AU_ex_phExRf project can not find the following function

706 Views
onlineit
Contributor II

Use the package NxpNfcRdLib in PN7462AU-FW_v05.02.01_Full to join the PN7462AU_ex_phExRf project can not find the following function:

.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldOff (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldOn (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_FieldReset (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_GetExtFieldStatus (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LPCD (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LoadProtocol_Initiator (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_RegCallBack (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_SetConfig (referred from phexrf.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_Exchg (referred from phexrf_15693.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_SetExchgFdt (referred from phexrf_15693.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_LoadProtocol_Target (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_MFC_Disable (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_ACFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_ShortFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgISO14443A_StandardFrame (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_PCD_ExchgMFC_Auth (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Receive (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Transmit (referred from phexrf_a.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_AutoColl (referred from phexrf_cm.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_DeInit (referred from phflashboot.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_Init (referred from phflashboot.o).
.\Objects\phExRf.axf: Error: L6218E: Undefined symbol phhalRf_SetIdleState (referred from phhalpmu.o).

Labels (2)
0 Kudos
3 Replies

392 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Xia Shuang,

I can compile this project well, see below:

pastedImage_1.png

I guess maybe you didn't import some projects into the same workspace.

Please check the following and compare with your workspace.

pastedImage_2.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

392 Views
onlineit
Contributor II

Hi Kan

      I do not want the libphhalRf_armcc.lib library

Tks.

Shuang

0 Kudos

392 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Shuang,

I am sorry, but so far just lib version is available.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos