Unable to connect dev board to NFC Cockpit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to connect dev board to NFC Cockpit

1,665件の閲覧回数
af0718
Contributor I

Hi there,

 

I have been trying to connect my PNEV7462C dev board to NFC Cockpit, but keep getting the same error message. I have tried uninstalling the driver & re-installing, and I have checked that there are no other applications running & connected to the dev board. Any help is appreciated. Thanks!2021-11-04 16_09_47-NXP NFC Cockpit v6.3.0 (Disconnected).png

ラベル(2)
0 件の賞賛
返信
1 返信

1,650件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 The firmware is the correct for the version of cockpit? Please kindly make sure it.

PS: please kindly refer to the document for  the updated firmware.

 Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信