The historical bytes is error in Mifare Plus S in SL0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The historical bytes is error in Mifare Plus S in SL0

826 Views
tony_liang
Contributor II

In the document AN10834,the historical bytes of Mifare Plus S in SL0 is:  C1 05 XX XX 00 35 C7,However,after I send the RATS command, I received the historical bytes witch show :  C1 05 21 30 00 77 C1,the first two bytes C1 05 is correct,but the last three bytes 00 77 C1 are not match with 00 35 C7,what's wrong ? 

0 Kudos
1 Reply

701 Views
eljeffo
Contributor III

Noticed the same with a MF Plus SE Card

0 Kudos