In the document AN10834,the historical bytes of Mifare Plus S in SL0 is: C1 05 XX XX 00 35 C7,However,after I send the RATS command, I received the historical bytes witch show : C1 05 21 30 00 77 C1,the first two bytes C1 05 is correct,but the last three bytes 00 77 C1 are not match with 00 35 C7,what's wrong ?
Noticed the same with a MF Plus SE Card