The difference between OM6716,599 and OM6716/434,599 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The difference between OM6716,599 and OM6716/434,599 ?

1,379 Views
mitorika
Contributor II

Hello sir :

we planed to purchase the OM6716 to read/write PCF7935, but we found the two type about OM6716 on NXP websit(see pic below). Could you help us to clearly point out the difference between two type in red mark.

Thank you.

pastedImage_1.png

0 Kudos
Reply
1 Reply

1,132 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

This is the information I received from a product manager:

The OM6716 (order number 935286468599) is our Transponder Evaluation and Development Kit 2 base station that supports the LF transponder HT2, HT2-E, HT-Pro, HT-Pro2, HT3, HT-AES.

                                              

OM 6716/434 (order number 935288366599) is the RF extension board for RKE/PKE, Supports the 434 MHz UHF frequency band as transmitter and receiver (LoPSTer). The OM6716/434 must integrate in the housing of OM6716.

pastedImage_1.png

 

Have a good day.

 

Best regards,

Ivan.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply