Temperature issue with PN5180A0HN/C1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature issue with PN5180A0HN/C1

862 Views
johnploeg
Contributor I

We have developed a PCB with a PN5180A0HN/C1   The LPCD feature is enabled (=default setting)  at his moment. Despite that the antenna matching circuitry needs some tuning we already can read the mifare cards.   So the chip is fully functional.

But there is an issue with the temperature. The chip is getting to hot. We measure a hot spot temperature on the casing of 98 C.

What can cause this dissipation? 

Does anyone had the same problem? 

The schematics are included.

There is some conflicting information regarding the capacitor on pin 17.  (VMID)

At this moment this pin is left open. 

According to the reference design in Application Note(AN11744)  a 100nF capacitor should be connected ground.

But according to the PN5180 Datasheet this pin is grounded??

(In the second attachment this can be seen)

Please give us some feedback on these matters.

Kind regards

John Ploeg

Labels (2)
Tags (2)
0 Kudos
1 Reply

698 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi John,

Please follow the reference design as the OM25180FDK does . Please refer to https://www.nxp.com/docs/en/application-note/AN11744.pdf  for details.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos