Tech question for SL3S1013FTB0,115

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tech question for SL3S1013FTB0,115

ソリューションへジャンプ
1,377件の閲覧回数
takashi_matsumu
Contributor II

Dear NXP team,

Thank you for supporting us.

This is Takashi from Digi-key.

I have customer question below;

Costumer is using SL3S1013FTB0,115 of NXP Semiconductors.
In his experiments, the sensitivity (minimum input power) was -7dBm,
though in the datasheet, typical value of minimum input power is -17.5dBm.
That is, the prototype is around 10dB worse than the data sheet value.

So he is inquiring of the advice for improvement


The measurement conditions are as the following.

R/W: The product of OMRON (EPC Gen2)
A matching circuit (loss=0.1dB) is used before the receiving circuit.
Modulation:
from R to Tag: DSB-ASK, PIE encode
from Tag to R: Miller sub-carrier, BLF: 400kHz, M=4
Communication speed:
from R to Tag: 60kbps
from Tag to R: 100kbps
Communication command:
Read command in the region of EPC code memory


Also, when using the product (Tag) of other company, communication error
did not occur in the unreceivable level for the prototype which uses NXP's IC.

Could you advise us about improving the performance of prototype ?


Thank you so much for your patience

Takashi

タグ(1)
1 解決策
1,271件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi,

 the read sensitivity is strongly depending on the used antenna form factor and design. The value in the datasheet is measured with a 50Ohm source impedance and shows the theoretical Pmin value you can achieve which this IC.

since we do not know the form factor there is not much we can say, if you can share the information please send them in a direct message so you dont share confidential information.

BR

Jonathan

元の投稿で解決策を見る

3 返答(返信)
1,271件の閲覧回数
takashi_matsumu
Contributor II

Hi Mr. Jonathan,

Thank you so much.

I forgot to put the file. 

pastedImage_1.png

Thank you for your patience.

Best Regards

Takashi

0 件の賞賛
返信
1,271件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi,

Sorry maybe I was not clear, my apologies, by this I meant the antenna design.

BR

Jonathan

0 件の賞賛
返信
1,272件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi,

 the read sensitivity is strongly depending on the used antenna form factor and design. The value in the datasheet is measured with a 50Ohm source impedance and shows the theoretical Pmin value you can achieve which this IC.

since we do not know the form factor there is not much we can say, if you can share the information please send them in a direct message so you dont share confidential information.

BR

Jonathan