I would like to use TagXplorer windows desktop software with ACR1281 reader, but I get message "Reader not supported" when try to connect.
In the supported readers list this reader model is included. So I don't understand why I'm getting this message.
Can anyone confirm that ACR 1281U-C1 works? Thanks!
No from my side
I can confirm that C1 works, I've tested it right now.
Trued the library you mentioned, it was able to connect but on reading ntag213tt, tag not available
,
I was testing it on NTAG 424 DNA chips.
Buddy do you have acr1281 sdk or any sample codes library you can share
No, I don’t use that.
I am facing the same issue , ACR 1281U-C2 not supported , the tagXplorer is hardcoded for specific reader I guess.
Dear Petr Prachar,
Please contact thecompany in charge of this ACR reader it might need a firmware update, since this is not an NXP reader is hard for me to tell whether this problem is related to TagXplorer. please confirm with the manufacturer of the reader.
Have a great day !
BR
Jonathan
Need some sample sdk codes for using the taplinx and writing ntag213TT messages.
How to start with reading writing on desktop
I'm having the same problem here.
I'm using ACR 1281U-C2.