TagXplorer is designed to work with the Reader SCL3711, but did not.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TagXplorer is designed to work with the Reader SCL3711, but did not.

4,369 Views
vikr
Contributor I

After opening the TagXplorer choosing the listet SCL3711 is possible, but trying to connect the SCL3711 failes with the message: "Reader is not supported !!!"

The SCL3711-Firmware is original by NXP as far as I know. Is there a newer firmware than from 2014 available?

vikr

0 Kudos
2 Replies

3,687 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Viktor Krön, sorry for the delay,  TagXplorer does not support SCL3711 for now, there are other readers supported,  in the release notes there used to be a note "SCL3711 not working stable" and im not sure why  it was removed but this is not supported by the moment, my apologies for the inconvenience this means to you and your project.

BR

Jonathan

0 Kudos

3,687 Views
vikr
Contributor I

Hi Jonathan Iglesias,

>Hello Viktor Krön<https://community.nxp.com/people/vikr>, sorry for the delay, TagXplorer does not support SCL3711 for now,

SCL3711 is still annonced as one oft he supported readers

>"SCL3711 not working stable"

the firmware is still the originally written and sold by NXP (to SCM)

bougt this NFC Tag Starter Kit by identive: http://www.identivenfc.com/en/nfc-software-development-kit-sdk/nfc-ndef-tag-editor-kit.htm because of the ducumented suppurt:there (after checking also the NXP-Website)

What shouldt I have made better?

any suggestions - exept buying another reader - are welcom

kindly regards

Viktor Krön

Von: Jonathan Iglesias

Gesendet: Dienstag, 27. März 2018 16:27

An: Krön, Viktor

Betreff: You have been mentioned by Jonathan Iglesias in Re: TagXplorer is designed to work with the Reader SCL3711, but did not. in NXP Community

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by Jonathan Iglesias<https://community.nxp.com/people/jonathaniglesias?et=notification.mention> in Re: TagXplorer is designed to work with the Reader SCL3711, but did not. in NXP Community - View Jonathan Iglesias's reference to you<https://community.nxp.com/message/999854?commentID=999854&et=notification.mention#comment-999854>

0 Kudos