Tag doesn't get detected on PN7150

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tag doesn't get detected on PN7150

1,728 次查看
chaitannya
Contributor I

Hello Everyone,

I am using PN7150 sbc with ncfDemoApp, that we are using with beagle bone black.
Here's the details of compilation.
Linux kernel version: 4.14.49-ti-r54
Gcc version: 6.3.0
I have used  --enable-alt & --enable-pn7150 options while configuration.
I have downloaded the latest code from git  as mentioned in the document AN11697 PN71xx Linux Software guide.
At present the tag is not getting detected by the sbc.

Here's the output of the previous NfcFactoryTestApp, which runs without errors.
----------------------------
NFC Factory Test Application
----------------------------
PN7150 NFC controller detected
Select the test to run:
     1. Continuous RF ON
     2. PRBS
     3. Standby mode
Your choice: 2
PRBS test:
 Select technology (A=0, B=1, F=2: A
 Select bitrate (106=0, 212=1, 424=2, 848=3: NFC Controller is now in PRBS mode - Press enter to stop
0

here's the log of nfcDemoApp


0:825:846 - NxpFunc:    startRfDiscovery: is start=1
0:828:185 - NxpFunc:    NfcAdaptation::HalWrite
0:831:200 - NxpFunc:    snepServerThread: enter

0:833:935 - 0:835:250 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=5
NxpFunc:    NfcAdaptation::HalCoreInitialized
1:171:312 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=5
1:176:652 - NxpFunc:    NfcAdaptation::HalWrite
1:183:847 - NxpFunc:    NfcAdaptation::HalWrite
1:196:902 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=5
1:198:674 - NxpFunc:    NfcAdaptation::HalPrediscover
1:199:933 - NxpFunc:    NfcAdaptation::HalWrite
1:205:288 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=5
1:210:373 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=9
1:212:221 - NxpFunc:    NfcAdaptation::HalCoreInitialized
1:547:032 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=4
1:552:702 - NxpFunc:    nfaConnectionCallback: event= 30
1:556:065 - NxpFunc:    nfaConnectionCallback: NFA_RF_DISCOVERY_STARTED_EVT: status = 0
Waiting for a Tag/Device...

1:559:969 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=9
1:561:915 - NxpFunc:    NfcAdaptation::HalCoreInitialized
1:891:212 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=4
1:898:726 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=9
1:901:824 - NxpFunc:    NfcAdaptation::HalCoreInitialized
2:232:275 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=4
2:240:467 - NxpFunc:    NfcAdaptation::HalDeviceContextDataCallback: len=9
2:244:071 - NxpFunc:    NfcAdaptation::HalCoreInitialized

Regards,

Chaitannya

标记 (2)
0 项奖励
回复
2 回复数

1,457 次查看
chaitannya
Contributor I

That tag is at present plain text, I have checked it with NFC dongle. Is anyone aware of the code ? 

0 项奖励
回复

1,457 次查看
jimmychan
NXP TechSupport
NXP TechSupport

DESFire documents are restricted. Please download the DESFire documents from https://www.docstore.nxp.com .

0 项奖励
回复