Some issue in operation of IIC,using nhs3152

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some issue in operation of IIC,using nhs3152

1,376 Views
liliao
Contributor II

Hi,

    In my solution, I need IIC communication. Here is my circuit:

22222222222222222222222.PNG

   And I add 10Ω resistance for protecting circuit. But When I run software, IIC I/O always go wrong. It's like the I/O port totally doesn't work.

111111111111111111111111111.PNG

  I know IIC port work in open-drain mode. But I don't know using 10Ω protection resistance.is ok or not.

  And when I use oscillograph to detect signal, I/O port always break down, unless I detect through 1K protection resistance.

  In communication, I find one possible problem that is START condition.

3333333333333.PNG

  If I neet to read data from sensor, I should re-start without stop signal. And I don't know IIC API founction could achieve this operation or not.

  By the way, I have communicated with sensor using stm32 in gpio imitation method. And it's a little difficult to do the same way in nhs3152, because I couldn't set timer  precise and steady.

  Until now, void I2C0_IRQHandler(void) function still doesn't work.

  Thanks for your reply.

  Sincerely,

  Li. 

Tags (4)
1 Reply

1,316 Views
liliao
Contributor II

Well, after I change pull-up resistance from 10MΩ to 4.7KΩ, IIC driver works.

Congratulation to myself.

Li