Some experimental questions about NXP3152

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Some experimental questions about NXP3152

723 次查看
1442284789
Contributor I

driesmoors

Hello, I would like to ask some questions about this Table 15, as follows:

1. What is the meaning of Res.

2. Is the Input Max the maximum that the chip can bear? However, the current in my experiment exceeds the Input Max by a large amount, and my experimental value is as follows:

PXAL3IR[}VVHH16E]U2ZT15.png@G2WNQVTW19F2T0@[}ZS{AR.png

0 项奖励
回复
2 回复数

653 次查看
driesmoors
NXP Employee
NXP Employee

Hi Qiang,

  • The last column indicates the resolution of the measurement. If your value changes with less that amount, the convertor may not be able to pick this up.
  • The minimum and maximum columns before that indicate the range in which this mode can be reliably used. The values will start to clip when the offered analog value is outside this range.

If your input signal is way larger than this range, you need to add a resistor to limit the current flowing to the chip.

Best,
Dries.

0 项奖励
回复

634 次查看
1442284789
Contributor I

hi,thank you for your reply.I also want to ask you for amplifier.If my  pressure sensor is only change 20_50ohm,Do I need  Additional amplifier to NXP3152?

0 项奖励
回复