Shielding PN5180

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,561件の閲覧回数
AlanSbor
Contributor II

Greetings to all residents of the forum.

Assembled the device in a bundle of ESP32 + CPU2104 + PN5180

IMG_20210419_211823 1600-1200.jpg

 General view of the device.

Power supply is stable, no noise or float. PN5180 - works at 3.3V.

Everything worked well on the mecket, but as soon as I began to carry out tests on my printed circuit board, it turned out that the interference from the PN5180 was very large.

The antenna is taken out through the connector separately. It was assumed that it would be possible to attach it to the bottom of the main board, but the labels are not readable even when tight to the antenna. At a distance of about 8-10 cm, they are read without problems.

I set up the RF section for the NXP soft program, but this did not solve the problem.
What can be wrong ?

An aluminum screen without a ground wire connection did not solve the problem.

I want to try shielding the radio with 3M 1194 shielded copper non-conductive tape.
Can anyone come across a similar one? Where to look ? What to re-read again?

Maybe there are recommendations from the shielding NXP company itself. 

0 件の賞賛
返信
1 解決策
4,495件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello.

Thanks for your update information. For the detail information please refer to the videos as the links.

URL:

https://www.nxp.com/video/nfc-antenna-design-2-antenna-matching:ANTENNA-MATCHING-VIDEO

https://www.nxp.com/video/nfc-antenna-design-3-metal-environment:ANTENNA-METAL-ENVIRONMENT-VIDEO

https://www.nxp.com/video/nfc-antenna-design-4-optimization-debugging:ANTENNA-DEBUGGING-VIDEO

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,511件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

On PCB, the bottom of filter circuit and matching circuit must be cleared. That's, you can't lay out the parts.

Please confirm it. Hope it help you.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信
4,501件の閲覧回数
AlanSbor
Contributor II

Hello,

I did not quite understand. Please tell me according to the scheme, what is wrong with it?

What part of the schema do you propose to clean and split?

I am attaching the diagram.27-04-2021 RF.jpg

 

0 件の賞賛
返信
4,496件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello.

Thanks for your update information. For the detail information please refer to the videos as the links.

URL:

https://www.nxp.com/video/nfc-antenna-design-2-antenna-matching:ANTENNA-MATCHING-VIDEO

https://www.nxp.com/video/nfc-antenna-design-3-metal-environment:ANTENNA-METAL-ENVIRONMENT-VIDEO

https://www.nxp.com/video/nfc-antenna-design-4-optimization-debugging:ANTENNA-DEBUGGING-VIDEO

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 件の賞賛
返信