Secondary bootloader examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Secondary bootloader examples

2,411 次查看
wouterdhondt
Contributor I

Hi

I'm looking for an example to create a secondary bootloader for the PN7462 (next to the default ROM USB bootloader). I have the regular application examples like the dooracces, HIF and poll examples. But can't find anything on creating a secondary bootloader. Any ideas or directions?

标记 (2)
0 项奖励
回复
1 回复

1,543 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Do you want to use PN7462AU UART and X-Modem for application update, in order to implement a secondary downloader?

In this case, you should refer to the  AN10995 - LPC1100 secondary bootloader (with software). The secondary Bootloader project described here is implemented with the M0 LPC and many concepts described could be reused also in PN7462AU secondary project.

Could you provide us with additional information on this request?

Regards,

Ivan.

0 项奖励
回复