SW3683-v05.07.01和SW3683-v05.19.00 PN7462AU_ex_phExCcid检测ISO15693卡的函数
phExCcid_Check_Presence_TypeV_Card(phacDiscLoop_Sw_DataParams_t *psDiscLoopParams)
总是失败,位于:
static void phExCcid_Handle_USB_Process(phacDiscLoop_Sw_DataParams_t *psDiscLoopParams)函数中,代码如下:
else if (gphExCcid_sUsb_SlotInfo.bCLSlotType == PH_EXCCID_USBCCID_CL_TYPE_V)
{
if (phExCcid_Check_Presence_TypeV_Card(psDiscLoopParams) != PH_ERR_SUCCESS)
{
gphExCcid_sUsb_SlotInfo.bAtrValid = 0;
phExCcid_UsbCcid_CardRemoved();
break;
}
}
请问NXP官方,这个bug如何处理?
the original example
Did you use the original example or is there any modification added by yourself? I may try to reproduce this issue here.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------