Reading Gemplus/Systag Ario 10 SL tag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reading Gemplus/Systag Ario 10 SL tag

601 次查看
vijo
Contributor III

Hi,

tag info: 13.56MHz 26K HF communication baud rate. Don't know the ISO. May be 15693 due to the 26KHz 1/4 pulse position coding.

Tried the various examples in UM10883 for the PN7462 demo board with no response.

Any ideas what to try next ?

Thanks in advance.

Best regards

Viggo

标签 (2)
标记 (1)
0 项奖励
1 回复

538 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Viggo Joergensen

Hope you are doing great, I would recommend using the advanced discovery loop example this switches from different protocols from :

   -ISO 14443A

   -ISO 14443B

   -Felica

   -ISO 15693

   - ISO/IEC 18000-3M3

other reason why you are not able to read this tag it might have some pricavy features enabled so you have to activate the card in other way, please check this if you still have issues check with the card manufacturer.

BR

Jonathan 

0 项奖励