Read/Write registers over I2C for NTAG I²C plus Explorer Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read/Write registers over I2C for NTAG I²C plus Explorer Kit

Jump to solution
2,121 Views
logansmall
Contributor I

Hi there,

I'm attempting to read/write the memory in the NFC tag using an mbed microcontroller over I2C.

First, I am attempting to read the session registers from the tag using the given protocol from the specification (see: read.jpg)

Using mbed, I have written a function that will attempt to do this, it puts a start condition on the bus, then the I2C address (0xAA), and gets an acknowledgement from the tag. (see: code.jpg)

However, when I place the session register address (0xFE), I do not get an acknowledgement (nak). In fact, I have tried every possible MEMA from 0x00 to 0xFF, and all do not receive a response.

I cannot figure out what is wrong, is there something I have missed? Any help would be appreciated.

Labels (1)
0 Kudos
Reply
1 Solution
1,713 Views
logansmall
Contributor I

This ended up being an issue with how mbed implemented i2c writes, no worries.

View solution in original post

0 Kudos
Reply
1 Reply
1,714 Views
logansmall
Contributor I

This ended up being an issue with how mbed implemented i2c writes, no worries.

0 Kudos
Reply