Question about NTAG I2C plus Flex Antenna Class6.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about NTAG I2C plus Flex Antenna Class6.

ソリューションへジャンプ
3,667件の閲覧回数
gxu
Contributor II

Hello,

We are doing a project with your NFC chip NT3H2111. In this project, NTAG I2C plus Flex Antenna Class6 was adopted.  We want to design a new PCB which includes this antenna Class 6, but we could only download a Gerber document about it . Could you please send us a PCB document about NTAG I2C plus Flex Antenna Class6? 

ラベル(1)
タグ(2)
1 解決策
2,929件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Actually the PCB document come along with the Gerber document, you may fetch it from http://www.nxp.com/documents/software/SW3646.zip. Anyway, I attached it here for your convenience and you should use EAGLE to open that file.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

9 返答(返信)
2,929件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello Kan,

I prefer 1 too, but I still haven't got layout for antenna for Eagle. I cannot import any file, which you recommended me.

Thank you.

Best Regards,

Vilem

0 件の賞賛
2,930件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Actually the PCB document come along with the Gerber document, you may fetch it from http://www.nxp.com/documents/software/SW3646.zip. Anyway, I attached it here for your convenience and you should use EAGLE to open that file.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,929件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hi,

these files really helped me too. But now, I want try PN7120 or PN7150, but I cannot find something like that for Eagle software. Please, could you help me? Have you got any similar files for PN7120 or PN7150? 

Thank you very much!

Best Regards,

Vilem

0 件の賞賛
2,929件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Vilem,

Please refer to the following for details.

PN7120:

https://www.nxp.com/downloads/en/board-support-packages/HW3739.zip 

https://www.nxp.com/downloads/en/board-support-packages/HW3346.zip 

PN7150:

https://www.nxp.com/downloads/en/board-support-packages/HW3560.zip 

https://www.nxp.com/downloads/en/board-support-packages/HW3561.zip 

Hope that helps,

Have a great day,
Kan

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,929件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello Kan,

thank you very much for the fast reply and for the links. I tried use it in eagle, but I cannot import the BRD files. Maybe, it is not for Eagle. I need mainly antenna for my design. 

And one additional question. Can I use external antenna - for example this: https://www.molex.com/molex/products/datasheet.jsp?part=active/1462360031_ANTENNAS.xml&channel=Produ...

Thank you.

Best regards,

Vilem

0 件の賞賛
2,929件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Vilem,

We have a NFC antenna dev kit available, NFC Antenna Development Kit | NXP , why not use this?

Have a great day,
Kan

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
2,930件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello Kan,

Thank you, it looks good for development. But I need something low-cost for small production, too.

I have two solutions:

1. PN7150 + own antenna on own PCB

2. PN7150 + cheap external antenna + own PCB for PN7150 only

Thank you.

Best Regards,

Vilem

0 件の賞賛
2,930件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Vilem,

Actually I prefer 1.

Have a great day,
Kan

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
2,930件の閲覧回数
gxu
Contributor II

Thank you very much!

gxu@zju.edu.cn

0 件の賞賛