基于QN9090T SDK2.6.4(DK6开发板)进行NFC相关开发:
需要的硬件环境:
1. QN9090 DK6开发板。
2. NFC读卡器PN7150插入到DK6开发板上。(目前还没有拿到PN7150,使用先使用带NFC的手机来进行调试测试吗?有涉及到ntag代码如何适配通用带NFC的手机?)
楼主您好,
如果您想使用手机来测试这个板子的NTAG功能的话。 可以下载手机版taginfo. 或者TAPlinx APP都是可以的。
希望这些信息能够帮助到您。
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
您好!
taginfo 已下载安装。
QN9090T SDK2.6.4里面的ntag例程 是NFC标签的哪种类型? 如下:
另外基于QN9090T的NFC ntag可以具体做哪些功能点应用(比如配对,使NFC reader读信息)?
您好,
这个可读的TAG 是tag2. 具体的应用您可以用tagxplore APP 去操作或者使用SDK里的TAG demo去操作。
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
您好!
用SDK2.6.4 ntag demo , 已经使用了手机APP 识别到是tag2 ,程序运行也正常。
代码运行打印提示如下截图:
现需要评估对QN9090T SDK2.6.4 NFC ntag demo移植到ble例程。 有没有相关可行性与具体移植参考说明或例子呢?
另外这个QN9090T sdk NTAG demo 有没有程序运行架构流程图呢? 类似如下这样的ble程序架构图:
帮忙看看 , 谢谢!
您好,关于这个相关的问题,我在您的另外一个帖子上有回复。
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
您好!
我们这边需要评估对QN9090T SDK2.6.4 NFC ntag demo移植到ble例程。 有没有相关可行性与具体移植参考说明或例子呢?
以上问题没有看到回复哦!
帮忙看看, 谢谢!