Problems doing updateBinary

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems doing updateBinary

1,630 次查看
larryansell
Contributor I

Problem doing updateBinary on ST25TA 8K.  I have been able to write using updateBinary only several times.   Most often I get a strange set of bytes.

For example:

I send 16 bytes using the NDEF updateBinary command after the NDEF Select file

0x2 0x0 0xd6 0x0 0x4 0x10 0x54, 0x77 0x61 0x73 0x62 0x72 0x69 0x6c 0x6c 0x69, 0x67 0x61 0x6e 0x64 0x74 0x68 

and I get back

0xf2,0x2,  

Which almost fits as a WTX but the bits 7 and 6 are not set.  So it's almost like a deselect?

Sometimes I get no response from the card.

Any insight into this would be greatly appreciated.

Thanks,

Larry

标记 (1)
0 项奖励
回复
4 回复数

1,510 次查看
harrybellen11
Contributor I

Can you please explain it a bit? I mean what's exactly you are facing and all such stuffs, so that I can guide you. Thanks and Regards, Harry Bellen.

0 项奖励
回复

1,510 次查看
larryansell
Contributor I

Hi Harry,

Thanks for your email!

It was explained to me that the f2 2 was in truth a WTX. I had been looking at the ST25TA64k doc(where the table was labelled S-Block detailed format), but in the corresponding table in the ST25TA2k doc, the table is labelled PCB field of the S-Block format) so that makes sense.

Now (with a different card) I am writing an 8 byte message successfully at offset 4 but when I try a longer 16 byte message I get no ACK/NAK. I’m suspicious that I need to zero the NDEF but when I tried overwriting the two bytes at offset 0, I once again got the no ACK/NAK. But when I changed my offset back to 4 (where I had been writing the 8 bytes successfully) I was once again able to write the 8 bytes.

I would be grateful for any guidance!

Thanks again,

Larry

0 项奖励
回复

1,510 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Could you please let me know which reader or frontend are you using? 

Regards, 
Estepahania

0 项奖励
回复

1,510 次查看
larryansell
Contributor I

Hi Estepahania,

I’m using a pn5180, with code modelled on the nxp reader lib.

Thanks,

Larry

0 项奖励
回复