PRH600 TX1 (32) & TX2 (30) Max Output Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PRH600 TX1 (32) & TX2 (30) Max Output Voltage

487 Views
luisfernando_sa
Contributor I

Hello,

Could you provide infomation about the max output voltage and current that TX1 and TX2 outputs can achieve?

VDD is connected to +5V. Additionally, a 125KHz Antenna (600uH; DC resistance < 25homs) is connected from TX1 to TX2 with DC blocking capacitors.

Any information you could provide will be really appreciated.

Best regards,

Luis Fernando Sandoval.

Tags (1)
0 Kudos
Reply
0 Replies