PNEV5180 : Connecting it to an external Antenna

cancel
Showing results for 
Search instead for 
Did you mean: 

PNEV5180 : Connecting it to an external Antenna

609 Views
harpoon
Contributor II

Hi all,

I am trying to figure out how I can connect the PN5180 (using the PNEV5180 development board) to and external amplifier, and then to an antenna.

The details :-

I have the EMVCo test bench with a tuned antenna (like a Poller-0 antenna) and wish to use the PNEV5180 to communicate with a card using this antenna.

While I have some ideas on how to wire up the TX, I am not too sure about the RX path back to the PNEV5180

Can someone provide some insights ?

Thanks.

0 Kudos
1 Reply

401 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, you may cut the OM25180 along the red line shown as below, and add the amplifier between these two parts.

pastedImage_1.png

Please note the matching circuit should be adjusted.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos